+++ E3.ETPrint
Designer-37462: Allow (customer-specific) attributes/properties as print text / for export
Designer-37466: Filter higher level assignment and location with wildcards
Designer-38211Switch of setup to WiX (Windows Installer XML) toolset
Designer-38650 M-Print Pro: The selected marker attribute value is not used, instead the attribute value from the .etc file is always taken.
Designer-30342 Needed attribute definitions shall directly be created in E3 project and not by using the script AddAttributes.vbs
--- Version 3.5.11 09.03.2021
Documentation Updates
--- Version 3.5.10 15.01.2020
Designer-33461 (Product) Diverse enhancements for export/import to/from Phoenix Contact PROJECT complete
--- Version 3.5.9 06.11.2019
Designer-34844 The option "Regular Exp." is deactivated when loading a configuration
Designer-34794 The command 'Save to M-Print PRO' interrupts with following error ''Part of the path "C:\Zuken\E3.ETPrint\%ALLUSERSPROFILE%\Zuken\ETPrint\ETPrint_M-PrintPRO_Importscript-1.mis" could not be found'
--- Version 3.5.8 02.07.2019
Designer-33461 (Product) Diverse enhancements for export/import to/from Phoenix Contact PROJECT complete
--- Version 3.5.7 22.03.2018
Designer-31059 Path for ETPrint.etc is written to the registry
--- Version 3.5.6 11.10.2017
Designer-30823 After ETPrint installation a directory "Weidmueller" is created on C:
Designer-30780 CSV files can't be buffered within the installation path
Designer-30646 (Product) Export to M-Print PRO; Change the functionality 'Print directly'
--- Version 3.5.5 05.04.2017
Designer-29480 No function of script AddAttributes.vbs from E3.ETPRINT 3.5.4
Designer-30020 A checkbox "Print directly" shall be added under 'local M-Print PRO installation path'
Designer-30019 When at 'M-Print PRO import script' the MIS file is not configured or not existing, only the CSV file (no ZIP file) shall be written instead of abort
Designer-29692 Convert all E3-Tools to supported .NET-Version
--- Version 3.5.4 26.10.2016
Designer-26760 Interface from E3.series to M-Print PRO
--- Version 3.5.3 29.04.2016
Designer-26973 Configurable connectors are not listed in E3.ETPrint when connectors of open sheets are selected 
Designer-24905 When using double level terminal blocks, the print output of the terminal numbers displays only the first level
--- Version 3.5.2 10.11.2014
Designer-25894 Data selection 'device' contains cable ducts and rails although there is a separate selection for this 
--- Version 3.5.1 05.05.2014
Designer-25096 Settings are incorrectly saved and read
--- Version 3.5.0 21.12.2012
AddOns-01400 Addons may not write data into the program files directory due to the compatibility with Windows 7
--- Version 3.4.0 13.09.2012
AddOns-01135 E3.ETPrint: Enhancement wishes for ET-Print
AddOns-01409 E3.ETPrint: Allow wildcards anywhere in the filter string
AddOns-01395 E3.ETPrint: Reasing the 'List' row in the'[RegularExpressionList]' section of the configuration file (.etc) is aborted after 256 characters
AddOns-01408 E3.ETPrint: additional attributes are not printed out
--- Version 3.3.0 05.07.2012
AddOns-01423 Alle Addons: Saved window settings not used if an older Addon version was installed
--- Version 3.2.0 14.09.2011
AddOns-01239 All AddOns: Windows position not stored in consistent folder
AddOns-01238 E3.ETPrint/ The controls are not where they should be upon initially starting under Windows 7
--- Version 3.1.0 18.07.2011
AddOns-01197 All Addons: 64 bit version for all Additional Tools
--- Version 3.0.0 01.06.2011
AddOns-01102 E3.ETPrint/ 'Zuken layout' missing when executing SETUP and software list displays entry without E3 logo
AddOns-01092 E3.ETPrint/ Some translations missing
--- Version 2.7.0 25.02.2011
AddOns-01005 All Addons/ Saving/Restoring window position
AddOns-01004 E3.ETPrint/ Changing fort of configuration file (.etc) to INI format
AddOns-00929 E3.ETPrint/ Outputting attribute as additional information
AddOns-00927 E3.ETPrint/ Filtering output file using attribute
--- Version 2.6.0 09.02.2011
AddOns-00983 E3.ETPrint: Adaptions for E3 x64
AddOns-00754 All Addons/AppDev: Digitally signing DLLs, EXE files etc
--- Version 2.5.0 26.02.2010
AddOns-00465 Documentation/Localization: E3.ETPrint
--- Version 2.4.0 18.12.2009
AddOns-00527 ETPrint: 'Multiply print data' section not clear
AddOns-00526 ETPrint: Data to be output not read from ETPrint.etc
--- Version 2.3.0 07.09.2009
AddOns-00387 E3.ETPrint: No labels found when only terminal number and DevDes selected
--- Version 2.2.1 02.09.2009
AddOns-00425 E3.ETPrint: Error with regular expression
AddOns-00417 E3.ETPrint: German documentation not updated
--- Version 2.2.0 22.07.2009
AddOns-00356 E3.ETPrint: Documentation not up to date
--- Version 2.1.2 23.06.2009
AddOns-00357 E3.Print: Display order of RefDes, assignment and location can't be set
--- Version 2.1.1 16.06.2009
AddOns-00343 E3.ETPrint: Last DevDes in project not output
--- Version 2.1.0 25.05.2009
AddOns-00307 E3.ETPrint: Distances between labels
AddOns-00247 E3.ETPrint:: Possibility to output the terminal numbers of terminal strip's terminals
AddOns-00321 E3.ETPrint: Error message when loading .etc files
AddOns-00306 E3.ETPrint: Defining first row of printout
--- Version 2.0.5 25.03.2009
AddOns-00244 E3.ETPrint: Values also in INCH
AddOns-00248 E3.ETPrint: Print preview displayed in German even with English interface
AddOns-00243 E3.ETPrint: Erroneous English interface / missing field description
--- Version 2.0.4 10.03.2009
AddOns-00234 ALL: Change all AddOns to a new 'ConnectToE3' function
--- Version 2.0.3 20.10.2008
AddOns-00131 E3.ETPrint: Adding 'Tube' and 'Hose' component types
--- Version 2.0.2 29.04.2008	
Prog-00657 E3.ETPrint: Enhancement by double labels filter