========================================================================
                         WEIDMUELLER Linux Real TTY Driver

                              README file

  Date: 18-04-2018
  Copyright (C) 2018 Weidmueller Interface GmbH & Co. KG. All rights reserved.
========================================================================
Content

1. Introduction
2. OS Supports
3. System Requirement
4. Procedure
5. Hardware Installation
6. Installing the Driver File
7. Mapping TTY Ports
8. Settings for Secure Real COM Mode
9. Remove Mapped TTY Ports
10. TTY Naming Rule
11. Removing the Driver
12. Modification of "secreal2d.cf"
13. Modification of Initializing Script
14. Add additional server
15. Limitation
16. Technical Support
------------------------------------------------------------------------
1. Introduction
    The purpose of this driver is to map SE-Converter serial port to host tty
    port. Using this driver, you can use SE-Converter serial port as local
    tty port.

2. OS Supports
    Please read VERSION.txt to check the support list.For other systems
    not in list, please visit official website to download corresponding
    drivers.

3. System Requirement
    To install this driver, you will need SE-Converter Server and one of
    the following system.

     -  kernel 2.4.x or 2.6.x or above and the kernel source package
     -  gcc-2.7.2.1 or above
     -  ld.so-1.7.14 or above
     -  libc.so-5 or above
     -  binutils-2.7.0 or above
     -  make-3.74 or above
     -  gunzip-1.2.4 or above
     -  gawk-3.1.1.9 or above
     -  openssl-1.0.0 or above (For Secure Real COM Mode only)

4. Procedure
    To map SE-Converter serial port to host tty port, you need to:
    1. Setup SE-Converter.
      Make sure the IP configuration is correct and you can access
      the SE-Converter (ping, telnet...) successfully and then configure 
      the SE-Converter serial port to Real COM Mode. 

    2. Install driver files into the host.
      Refer to "6. Installing the Driver File" below for details.

    3. Map SE-Converter serial port to host's tty port.
      Refer to "7. Mapping TTY Ports" below for details.

5. Hardware Installation
    Before proceeding with the software installation, make sure you 
    have completed the hardware installation, as described in an 
    earlier chapter of this manual. 
    
    The default IP address for SE-Converter Server is 192.168.127.254.

    For SE-Converter Wireless series, the default IP address of the Ethernet
    interface is 192.168.126.254, and the default IP address of the
    Wireless LAN interface is 192.168.127.254.

    !!!!!!!!!!!!!!!!!!!!!!!!!!!! NOTE !!!!!!!!!!!!!!!!!!!!!!!!!!!!
      After installing the hardware, you MUST configure the 
      SE-Converter operating mode to Real COM Mode. If you want to  
      communication with security, please enable secure mode
      in both SE-Converter and Real TTY configuration.
    !!!!!!!!!!!!!!!!!!!!!!!!!!!! NOTE !!!!!!!!!!!!!!!!!!!!!!!!!!!!

6. Installing the Driver File
    a. Copy the driver file from the products CD-ROM or Weidmueller website.
    b. Log in to the console as a super user (root).
    c. Execute "cd " to change to the home directory.
    d. Copy the driver file secreal2xx.tgz to the home directory.
    e. Execute "tar xvfz secreal2xx.tgz" to copy all files into the system.
    f. Execute "./weidmueller/wminst" for Linux kernel 2.4/2.6.x.
	
    !!!!!!!!!!!!!!!!!!!!!!!!!!!! NOTE 1!!!!!!!!!!!!!!!!!!!!!!!!!!!!
	  For Red Hat AS/ES/WS and Fedora Core1, extra argument is 
	  needed: # /tmp/weidmueller/wminst SP1 
    !!!!!!!!!!!!!!!!!!!!!!!!!!!! NOTE 1!!!!!!!!!!!!!!!!!!!!!!!!!!!!
    
    !!!!!!!!!!!!!!!!!!!!!!!!!!!! NOTE 2!!!!!!!!!!!!!!!!!!!!!!!!!!!!
	  If you use driver in 64-bits environment, you may use extra 
	  argument m64, SP1_m64 or mppc64.(the SP1_m64 is for Red Hat 
	  AS/ES/WS and Fedora Core1 64-bits environment; The mppc64
          is for PowerPC64 only.) Ex.
	  # /tmp/weidmueller/wminst m64
    !!!!!!!!!!!!!!!!!!!!!!!!!!!! NOTE 2!!!!!!!!!!!!!!!!!!!!!!!!!!!!

    g. The shell script will install the driver files automatically.

    After installing the driver, you will be able to see several 
    files in the "/usr/lib/secreal2/driver" folder, including:

     - wmaddsvr (Add Server, map tty port)
     - wmsetsec (Set secure communication mode)
     - wmdelsvr (Delete Server, un-map tty port)
     - wmloadsvr (Reload Server)
     - wmuninst (Remove tty port and driver files)

    At this point, you will be ready to map the SE-Converter serial port to 
    the system tty port. See "7. Mapping TTY Ports" below for detailed 
    instructions.

7. Mapping TTY Ports
    7.1 Real COM Mode
	  Before mapping tty ports, you must set the operation mode of your 
      SE-Converter to Real COM Mode. We provide two ways to map tty ports.
   
    a. Mapping tty ports automatically
      After logging in as a super user, enter the directory 
      "/usr/lib/secreal2/driver" and then execute "wmaddsvr" to map the 
      target SE-Converter serial port to the host tty ports. 
      The syntax of "wmaddsvr" is:

       wmaddsvr [SE-Converter IP Address] [Total Ports] ([Data port] [Cmd port])

      Example 1:
       # cd /usr/lib/secreal2/driver
       # ./wmaddsvr 192.168.3.4 16

      Example 2:
       # cd /usr/lib/secreal2/driver
       # ./wmaddsvr 192.168.3.4 16 4001 966

      In Example 1, 16 tty ports will be added, all with IP 192.168.3.4, 
      but with data ports equal to (950, 951, ..., 965), and command ports 
      equal to (966, 967, 968, ..., 981). 
      
      In Example 2, 16 tty ports will be added, all with IP 192.168.3.4, 
      but with data ports equal to (4001, 4002, ..., 4016), and command 
      ports equal to (966, 967, 968, ..., 981). 
      
    b. Mapping tty ports manually
      After entering the directory "/usr/lib/secreal2/driver", you can modify 
      "secreal2d.cf" to map SE-Converter serial ports to tty ports, and then execute 
      "wmloadsvr" to activate the modifications.
      
      The following tasks will be performed:
     
       - Modify secreal2d.cf
       - Create tty ports in the directory "/dev" with major & minor number 
         configured in "secreal2d.cf"
       - Stop and then restart the driver.

	7.2 Redundant COM Mode
	  Before mapping tty ports, you must set the operation mode of your 
      SE-Converter to Redundant COM Mode and make sure your device is CN2600 
      series. 
	  We provide a new command to map tty ports to be Redundant COM Mode.

    a. Mapping tty ports
      wmaddsvr -r [SE-Converter IP1 Address] [SE-Converter IP2 Address] [Total Ports]

	  Example :
		# cd /usr/lib/secreal2/driver
	    # ./wmaddsvr -r 192.168.32.134 192.168.126.123 16
		
	  In Example, 16 tty ports will be added, all with 
	  IP1 192.168.32.134 and IP2 192.168.32.126, but with data ports 
          equal to (950, 951, ..., 965), and command ports 
          equal to (966, 967, 968, ..., 981).

8. Settings for Secure Real COM Mode
   a. Check necessary library for Secure Real COM Mode
     User should visit https://www.openssl.org or the official website
     of your Linux distribution to install openssl library libssl.so.

     A simple way to test if you have libssl.so, please type 'ldconfig -p'
     command and the result should like below example.

       # ldconfig -p | grep libssl.so
            libssl.so (libc6) => /usr/lib/i386-linux-gnu/libssl.so

   b. Enable or disable the secure mode
     A script wmsetsec is used to set secure mode enable/disable.
	
     !!!!!!!!!!!!!!!!!!!!!!!!!!!! NOTE !!!!!!!!!!!!!!!!!!!!!!!!!!!!
     This function is support SE-Converter 6000 series only.
     If your model is not SE-Converter 6000 series, you could ignore this chapter.
     !!!!!!!!!!!!!!!!!!!!!!!!!!!! NOTE !!!!!!!!!!!!!!!!!!!!!!!!!!!!
	
     The syntax of "wmsetsec" is:
    
     wmsetsec
    
     Example:
       # cd /usr/lib/secreal2/driver
       # ./wmsetsec

9. Remove Mapped TTY Ports
    As with the "8. Mapping TTY Ports" task, we provide two ways to remove
    mapped tty ports:
   
    a. Remove the mapped tty ports automatically
      After logging in as root, enter the directory "/usr/lib/secreal2/driver" 
      and then execute "wmdelsvr" to delete a server. 
      The syntax of "wmdelsvr" is:

      wmdelsvr [IP]  ; For Real COM mode.
      wmdelsvr [IP1] ; For Redundant COM mode.
      
      Example:
       # cd /usr/lib/secreal2/driver
       # ./wmdelsvr 192.168.3.4
           
      If you don't include the IP address in the command line, a numbered 
      list of IP addresses for servers currently installed, along with the 
      total number of ports for each server, will be listed on the screen.
      To remove the tty ports for a particular server, type the number next 
      to the server's IP address and then hit Enter. The following tasks 
      will be performed:
    
       - Modify the secreal2d.cf 
       - Remove the relevant tty ports in directory "/dev"
       - Stop and then restart the driver.  
      
    b. Remove the mapped tty ports manually
      After entering the directory "/usr/lib/secreal2/driver", you can 
      modify "secreal2d.cf" to delete servers and ports manually, and then 
      execute "wmloadsvr" to activate the modifications.

	  
10. TTY Naming Rule
     The tty name of the Real TTY driver is configured in secreal2d.cf. 
     The pre-defined tty name is ttywXX, and the callout name is cuwXX. 
     The naming convention is illustrated as follows:

     SE-Converter        TTY Name              Callout Name
     1st(4port)       ttyw00 - ttyw03         cuw00 - cuw03
     2nd(8port)       ttyw04 - ttyw0b         cuw04 - cuw0b
     3rd(16port)      ttyw0c - ttyw1b         cuw0c - cuw1b
     4th(8port)       ttyw1c - ttyw23         cuw1c - cuw23
     ...(etc.)

     !!!!!!!!!!!!!!!!!!!!!!!!!!!! NOTE !!!!!!!!!!!!!!!!!!!!!!!!!!!!
	   1. Callout Device is obsolete in Linux 2.6. That is, you 
	      cannot open Callout Device on Linux 2.6.
	   2. ttyw0 - ttyw9 or some tty names represented by decimal
	      number are created for kernel compatibility reason. User
	      must use tty port name combine with hexadecimal digits
	      for correct operation.   
     !!!!!!!!!!!!!!!!!!!!!!!!!!!! NOTE !!!!!!!!!!!!!!!!!!!!!!!!!!!!
 
11. Removing the Driver
     Removing the driver will remove all driver files, mapped tty ports, 
     and unload the driver. To do this, enter the directory 
     "/usr/lib/secreal2/driver", and then execute "wmuninst" to uninstall 
     the driver. This program will perform the following tasks:
    
      - Unload the driver.
      - Delete all files and directories in "/usr/lib/secreal2"
      - Delete directory "/usr/lib/secreal2"
      - Modify the system initialization script file.

12. Modification of "secreal2d.cf"
     !!!!!!!!!!!!!!!!!!!!!!!!!!!! NOTE !!!!!!!!!!!!!!!!!!!!!!!!!!!!
       "secreal2d.cf" is the driver configuration file. Please 
       backup this file before making any modification.
     !!!!!!!!!!!!!!!!!!!!!!!!!!!! NOTE !!!!!!!!!!!!!!!!!!!!!!!!!!!!

     The configuration file is named "secreal2d.cf" in directory
     "/usr/lib/secreal2/driver", all relevant information about
     mapped tty ports will be appended in this file. you are
     allowed to modify this file if you want to modify the setting
     manually.

     We illustrate some circumstances that you may encounter in the
     following section. Please read the CAUTION section before
     reading the section a and section b.

     [CAUTION]:
      In modifying "secreal2d.cf",
      1. Please don't type any space or [TAB] character between
         ttymajor and '=' and the number.
      2. Please don't type any space or [TAB] character between
         calloutmajor and '=' and the number.
      3. Please type only one [TAB] character to seperate the 
         columns of the settings.

     a. Major Number
       The Real TTY driver allows you to change the major number
       manually. So you can modify the major number in "secreal2d.cf".
       And then execute the program "wmloadsvr" with an
       argument "module". For example:

        # cd /usr/lib/secreal2/driver
        # ./wmloadsvr module

       The driver will remove the module and reload the driver with
       new major number configured in "secreal2d.cf". The connections
       will be closed after the new driver is loaded.
       The following actions will be performed.

        - Unload driver.
        - Re-create all device files configured in "secreal2d.cf"
          with new major number.
        - Load driver.

     b. TTY Name & Callout Name
       Similar to the previous section, modification of tty name and
       callout name will be activated after executing "wmloadsvr".
       Since we do not modify the major number, so the driver will not
       be reloaded. We merely need to execute "wmloadsvr" to reload
       the settings without any argument.
       The following actions will be performed.

        - Close connections.
        - Re-create all device files configured in "secreal2d.cf".
        - Open the connections.

13. Modification of Initializing Script
     a. For Red Hat
       The script file "/etc/rc.d/rc.local" will be executed when Linux
       boots up. Therefore the driver will append the instructions which
       is used to load Real TTY driver in the script file.

     b. For Debian
       All script files in directory "/etc/init.d/" will be
       executed when Linux boots up. The Real TTY driver will copy
       the initialinzing script file to that directory and update
       the symbolic link to the script so that if the system boots
       up next time, the system will perform the relevant actions
       which are described in the script.
	   
           Caution:
             If the Debian system boots without SE-Converter driver loaded, please
             execute following command with root administration to resolve this
             problem:
	   
	       # update-rc.d secreals defaults

             Starting with Debian 6.0, the insserv command is used instead as
             below instruction.

               # insserv /etc/init.d/secreals

     c. For SuSE
       The initializing script file in SuSE is "/etc/rc.d/boot.local".
       The driver will append the instructions which is used to load
       Real TTY driver in the script file.

     d. For Gentoo
       The initializing script file in Gentoo is "/etc/conf.d/local.start".
       The driver will append the instructions which is used to load
       Real TTY driver in the script file.

14. Add additional server
     Step 1     
       Modify "secreal2d.cf" file to add additional server, or remove unused 
       server. User can use vi or any edit to modify it. It's a text file.
       For more configuration information, please take a look
       at secreal2d.cf file. We put detail decription on it.

     Step 2  
       Find the proccess id (PID) of program "secreal2d".
        # ps -ef | grep secreal2d

     Step 3  
       Update configuration of weidmuellerttyd program.
        # kill -USR1 PID
       (ex. if "secreal2d" PID = 404, "kill -USR1 404")

     Finish : You have finished to add additional server, 
              or remove unused server.
     
     [CAUTION]: 
	Please use the "wmaddsvr" to generate a temporary file for secreal2d.cf
	and follow the temporary file to modify "secreal2d.cf" if user don't 
	know how to modify the "secreal2d.cf" file .
	
	User can reference chapter 12 to understand the detail.
	
15. Enable background polling feature
	If you don't want your program been blocked when open tty port with SE-Converter
    not exist, you should enable this feature. This feature will polling SE-Converter
    device in background to eliminate the time your program been blocked.
       
    Following steps shows how to enable this feature

    a. Copy the driver file from the products CD-ROM or Weidmueller website.
    b. Log in to the console as a super user (root).
    c. Execute "cd " to change to the home directory.
    d. Copy the driver file secreal2xx.tgz to the home directory.
    e. Execute "tar xvfz secreal2xx.tgz" to copy all files into the system.
    f. Execute "./weidmueller/wminst polling".
	
16. Limitation
     1. Redundant COM Mode
	SE-Converter driver needs ONE minute the most to synchronize with SE-Converter device
	after the LAN port resumes connection.
	Therefore, during the maximum one minute synchronization if any one
	network connection loses again, data lose might happen. 

17. Technical Support
     If you have any technical questions, please send your question by
     the following ways with detail description of the symptom.

     Email: support.automation@weidmueller.com

-End-